Hello,
I am looking to drive a Bridgelux (BXRC-50C4001-B-74-SE) COB but have been having issues with the calculations for the inductor etc., mostly because the equations are based off of the "resistance" of an individual LED in a series circuit. I've contacted Bridgelux regarding the "resistance" value but they have not given me information requested. I did send a Bridgelux application engineer my circuit and he said it "should" work but... Now, I have recently come across the evaluation board design, but it does not match the boost circuit application note from the spec sheet... Could someone take a quick look at my circuit? I can send a screen shot of what I've got done - the board is already made but after seeing the mosfet on the evaluation board I fear I may have under spec'd the one I picked..
Thanks,
Shane