This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: CEDV parameter calculator

Part Number: BQ4050
Other Parts Discussed in Thread: GPCCEDV

Hi everyone, 

I have one issue concerning the CEDV parameter process in 'CellTermV'. The battery (2Series) has a set termination voltage of 3.2V=3200mV. However, in the Hightemp_highrate.csv file, the actual termination voltage falls above 3200 mV, which is 3307 mV. My concern is whether I shall use 3200 mV or the actual 3307 mV?

  • If your cell termination in the log is higher than the actual terminate voltage used in the parameters, you will be unable to calculate the CEDV paramters with GPCCEDV. I would suggest that you re-test and dsg the cell to slightly below 3.2V for generating your CEDV parameters.