Other Parts Discussed in Thread: BQ24610, , BQ76925
I'm actually using the BQ7791501 version of this part in a 5S configuration.
This particular chip offers and OV setting of 4.25V. For my 5S configuration, I am charging them up to 4.15V (20.75V for the whole pack) using a BQ24610 based circuit. My problem is that once the pack gets fully charged, I can remove it from the charger and find that the CHG pin has gone low (by the action of removing it from the charger). Connecting a 1A resistive load to the battery restores the CHG pin high but upon removing the load, the CHG pin goes low again. If I allow the battery to drain to approx. 20.5 or lower, this problem is not present. The main problem this presents is that if I remove then reinsert the battery into the charger, the charger faults outs thinking that no battery is connected.
For now, I'm assuming it is an OV fault since I have no way to absolutely verify none of the other CHG disable qualifiers are taking place (OT, UT, etc.). My OC set points are quite high (Rsense is 1.5milliohm) so I can't see it being that. I've tried capturing an overvoltage event with an oscope connected to the battery but I'm not seeing anything come that close to 4.25V (21.25/pack). The cells are balanced to within 10 mV. I have numerous 5S packs using several 18650 cell mfr's (sony, samsung, LG, Molicel) and they are all doing the same thing. It's as if there is some "glitch" taking place when I remove the load that I haven't been able to capture yet.
Thoughts?