This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65251: Accuracy over full temperature range (-40°C to +125°C junction temperature)

Genius 12865 points
Part Number: TPS65251

Hello Team,

may I ask you for the accuracy of the internal reference over the whole temperature range (Vin = 12V), please?

The data sheet only specifies the accuracy of the feedback voltage at Vin = 12V, Tj = 25°C with 0.8V +/- 1%.

Thanks and Best Regards,

Hans