This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS4H000-Q1: Behavior of CS & CL pin

Part Number: TPS4H000-Q1


Dear all.

CL pin and CS pin are set for current sensing and limit per channel.
For example, if you set CS = 300 mA and CL=400 mA respectively and use 350 mA on the selected channel,

when I calculate using eq.9 on the datasheet, is it correct that the fault is kept high because the Vcs(h) is not reached?

Thanks.