Other Parts Discussed in Thread: TPS23754
I have found limited discussion about the TI TPS23756 and 802.3at ("PoE+") compliance. Apparently, the negotiation for 802.3at involves two (here simplified) steps:
1. A primary voltage/current hardware negotiation, to determine if power is necessary on the port.
2. A secondary hardware OR software (LLDP) negotiation, to determine how much power is necessary on the port.
We have had no trouble with our product on Cisco SG300 series switches, but we are recently having trouble with our product negotiation power properly with the Cisco Catalyst 2960-X series switches. I saw one previous discussion about this same series of switch (linked to this thread). We are working with Cisco support to try to determine why, but this discussion led to investigation into the PoE IC that is used in the design of our product.
If the PSE can support either hardware or software negotiation (but does not have to support both), and the PD (our device using the TI TPS23756) has to support both -- my question is whether the TPS23756 DOES support both hardware and/or software (LLDP) negotiation. In our investigation, this seems to be one of the few reasons why it might work on one switch but not the other.
Our product definitely uses more than the standard 802.3af (15.4W) of power, and we require the higher power of an 802.3at Class 4 PSE port.
Thanks in advance for any help from the community!
Neil