Other Parts Discussed in Thread: DCV010505
Hi,
I made a circuit that uses DCV010505D to get isolated -/+5v output from +5V USB power. When I soldered everything and tested, I found the output was about -/+2V at no load. I don't have the 2.2uF capacitor at the current moment so I paralleled two 1uF ceramic capacitors for the input pin. I don't know if the issue is the wrong capacitor or others. I'm going to buy the 2.2uF capacitor and try it again. But I read that someone has a similar issue from this thread and I wonder whether they have resolved their issue or not. Look forward to your reply, thank in advance.
Thanks
Rui