This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5067: Review of LM5067 Design calculation for 20A and 12A current

Part Number: LM5067
Other Parts Discussed in Thread: TPS23521, CSD19536KTT

Hi,

We are using LM5067 negative hotswap controller IC in -48V power supply rail for 20A and 12A operating current. The design calculation sheet for LM5067 is attached herewith. We encountered an error while designing calculator sheet (please see row#62, column no. F). Is it due to the wrong components selection?? Kindly review it and give us your best possible solution for this.

Thank you.

Regards,

Nadim Ahmed

C-DOT, DelhiCopy_LM5067_Design_Calculator_20A.xlsxCopy_LM5067_Design_Calculator_12A.xlsx

  • Hi Nadim Ahmed,

    Welcome to E2E!

    I will review the sheets and get back to you.
    Can you share your project details.

    Best Regards,
    Rakesh
  • Hi Nadim Ahmed,

    Can you check with stronger FET something like PSMN4R8-100BSE. Else, we need to add dvdt startup circuit at GATE. In the later case, I prefer and suggest to use new device TPS23521, which offers more flexibility.

    Can you have a look at TPS23521 and let me know your opinion

    Best Regards,
    Rakesh
  • Hello Mr. Rakesh,

    Thank you for the response. Could you please guide us to select RDS(on) resistance at Tj, DC temperature. As per design calculation sheet for RDS(on) = 4.8 mili ohm the required Tj,DC is 110 degree C, while as per datasheet of PSMN4R8-100BSE, the drain source on-resistance RDS(on) = 4.8 m ohm at Tj,DC=25 degree C. Now, if the value of RDS(on) @ 110 degree C (from datasheet) is placed in calculator sheet, the Tj,DC   temperature automatically changes, since Tj,DC is dependent on RDS(on). Please clarify this.

    Regards,

    Nadim Ahmed

  • Hi Nadim Ahmed,

    It needs several iterations. Please follow video training.ti.com/.../1133673 and let me know if you still have questions.

    Best Regards,
    Rakesh
  • Dear Mr. Rakesh,

    The design calculation sheet for 20A and 12A operating current are attached. Kindly review these. Here, below are the few points that need to be clarified.

    (a)   As per datasheet the thermal resistance Rθ,JA = 50 K/W with MOSFET minimal footprint. However, the design calculation are done with Rθ,JA = 30 K/W and 40 K/W for 20A and 12A current respectively. Is it possible to have reduced Rθ,JA for MOSFET??

    (b)   For 20A operating current, it is difficult for us to set RDS, ON and TJ, DC parameters using a single MOSFET even with reduced Rθ,JA=30 K/W. Therefore, the design calculation is shown with 2 MOSFETs in parallel. But, due to space constraint in our PCB, we can not use dual MOSFET config. Is it possible to have the design with single MOSFET for 20A operating current??

    Thanks & Regards,                                                                                                                                                                                                                                                                                                                            NADIM AHMED, C-DOT, New Delhi

    LM5067_Design_Calculator_20A.xlsxLM5067_Design_Calculator_12A.xlsx

  • Hi Nadim Ahmed,

    (a) Rθ,JA = 50 K/W is with Minimum footprint. Increasing PCB heat sink area will help to reduce Rθ,JA.

    (b) you can go for Low Ron FET like CSD19536KTT and reduce fault timer capacitance to meet SOA margin.


    Best Regards,
    Rakesh
  • Hi,

    Thank you for the clarifications.

    The design calculation of LM5067 with low Ron FET like CSD19536KTT and reduced fault timer capacitance fails to meet the SOA margin. Therefore, we are planning now to use TPS23521 for 20A operating current as you suggested earlier.

    The design calculation sheet for TPS23521 is attached. Kindly review it and give us your feedback. Kindly also tell us whether we need heatsink for the transistors in this design.

    Regards,

    Nadim Ahmed

     TPS2352X_Excel_Tool_Baytop-20A.xlsx

  • Hi Nadim Ahmed,

    Even with TPS23521 device, 20A solution with a single FET is not possible because the temperature rise in steady state is determined by the FET Rds_on.

    If you leave Q2 blank in the design calculator, it pushes the Tj of Q1 to 177C

    The advantage of TPS23521 over LM5067 is at higher currents where multiple FETs are needed. TPS23521 allows single stronger SOA FET for Q1 and multiple "low Ron" FETs for Q2 there by reducing overall solution size and cost. Please refer application note for more details http://www.ti.com/lit/an/slvae07/slvae07.pdf

    So for your design, two FETs will be needed irrespective of the controller

    Best Regards,

    Rakesh

  • Hello,

    The design calculation for both the LM5067 and TPS23521 for 20A current are attached. We have used 2 MOSFETs for both the cases.

    For device TPS23521 if we use Q2 transistor along with Q1 the steady state junction temperature reaches 1280C, while for LM5067 the steady state junction temp. is 960C. Do we need hitsink for MOSFETs in the TPS23521 H/S circuit, since the design is with Rθ, JA=45 K/W which is only 5 K/W less than minimum footprint Rθ, JA i.e. 50 K/W.

    Kindly review both the designs (i.e. LM5067 and TPS23521) and suggest us which one would be the better solution.

    Regards,                                                                                                                                                                                                                                                                                                                                    Nadim1374.TPS2352X_Excel_Tool_Baytop-20A.xlsxLM5067_Design_Calculator_20AF.xlsx

  • Hi,

    The ambient temp is entered differently in the two designs. Is it 75C ? If yes - it will bring down the steady state junction temperature to 118C in TPS23521 design.
    I suggest to proceed with TPS23521 solution as it helps to scale up for your future high current designs. You would require, more PCB area as heat sink to lower Rθ, JA. Please use at least 1-inch2 PCB area dedicated for FETs however I feel the generated heat will spread to the adjacent PCB area and help especially if the board size is of decent size.

    Best Regards,
    Rakesh
  • Hi,

    Do you have any follow up questions?

    Best Regards,
    Rakesh
  • Hi,

    I hope you concluded your design. Please close this thread as resolved, If you do have any follow up questions, please feel free to reopen.

    Best Regards,
    Rakesh