This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24079T: SYSOFF to turn disconnected BAT to VOUT follow up

Part Number: BQ24079T


Hi TI!

Related to this post: e2e.ti.com/.../656891
Is the quiscent current of the BQ24079T higher than 6.5uA during SYSOFF when there is load on the OUT pin? I see in the datasheet that the test condition for the 6.5uA is given during "no load on OUT pin": I wonder if there is a reason that this is stated?
This could be useful information if the BQ24079T is used as a power switch to disconnect the battery to lower OFF current consumption.