This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Energy Rollover during charge

Part Number: BQ34Z100-G1

Hi,

We use golden image 25.6V 64Ah for Li-Ion battery with chemical 0463 validated by supplier on BQ34Z100-G1 and are faced to energy rollover.

we use current scale of 4 and design energy scale of 2 as design capacity is divided by 4 so 16Ah and design energy is 25600mWh= 3.2V x 16000ma / 2.

As you can see in attached file, especially on "end of charge GI" file, as the SOC is going to 100% we have huge gap on Available Energy and Remaining capacity.w

we noticed with this GIO that during first start, SOC was 70% instead he was supposed to be 95%.

Could you please help us as this problem stuck some products in our clients hands.

Many thanks

Renan

HET_LiFe_25.6V_64Ah_GI.zip