This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90160A: fusion power design online

Part Number: UCD90160A

Hellow,

we used the UCD9016A to control the power rail sequences and monitor the voltage, but some pins can not been configured. the note is shown below.

MONITOR_CONFIG write Pin 1 MON1: Rail #11, Type Voltage; Pin 2 MON2: Rail #12, Type Voltage; Pin 3 MON3: Rail #13, Type Voltage; Pin 4 MON4: Rail #1, Type Voltage; Pin 5 MON5: Rail #2, Type Voltage; Pin 6 MON6: Rail #3, Type Voltage; Pin 55 MON7: Rail #4, Type Voltage; Pin 56 MON8: Rail #5, Type Voltage; Pin 57 MON9: Rail #6, Type Voltage; Pin 58 MON10: Rail #7, Type Voltage; Pin 59 MON11: Rail #8, Type Voltage; Pin 62 MON12: Rail #10, Type Voltage; Pin 63 MON13: Rail #9, Type Voltage; Pin 50 MON14: Rail #14, Type Voltage; Pin 52 MON15: Rail #15, Type Voltage; Pin 54 MON16: Rail #16, Type Voltage [0x2A2B2C202122232425262729282D2E2F] on UCD90160A @ PMBus Address 65d error: NACK

and our configuration screen is enclosed. please help to resolve it. thanks!

Fang Youxiang

UTStarcom

Configuration screen.docx