This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23523: Review Required

Part Number: TPS23523
Other Parts Discussed in Thread: CSD19536KTT, CSD19532Q5B

Hello ,

We are planning to use Part# TPS23523 in our design for 20A operating current at negative 48VDC.
Below are our queries, please clarify :

1)What should be the drain pad area for mosfets to mount the heat sink aiming to reduce Rtheta,ja(Row#35, in the attached sheet) to 40?. Because as per datasheet value of Rjtheta is 62.

2) Weather the heat sinks are required for both the mosfets(part#CSD19536KTT
and part#CSD19532Q5B) ?
If required , kindly provide the details.

3) In the design sheet,at Row#39 Tj(max) for the Q1 is 124 degree centigrade. can Q1 withstand at this temperature?

The design calculation sheet is attached for your review.
Kindly provide the feedback at the earliest.

2211.TPS2352X_Excel_Tool_Baytop-20A.xlsx