This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
As below datasheet shows the "Minimum input pulse width that changes the output". Could you please help provide the max and min value of this parameter? Thanks a lot.
Wilson
Thank you, Richard, you answer helps me a lot. More questions need you warm support.
In my customer' application, the Vin varies in a large range and may reach the minimum input pulse width. So they want to know this parameter and then, limit the PWM in software level.
So to simplify my question, could you please provide:
1. The min high-level width of input that could change output;
2. The min low-level width of input that could change output.
My customer will limit the min on time and min off time in software through above two parameters, in their Solar optimizer.
Thanks in advance!
Best Regards!!!
Wilson
Hello Wilson,
For the minimum width high level transition and low level transition, the response is typically the same for high going signal and low going signals which is 10ns based on bench testing. For settings to guarantee operation we recommend the datasheet specification which is 50ns.
Let us know if this answers your question, or you can post additional questions on this thread.
Regards,
Richard Herring