Other Parts Discussed in Thread: LM25141
Hi,
with the below LM25141 converter we experience unexpected behaviour. Input voltage is 10..30V, output should be 5V (~10A). The circuit has a load-side capacitor with 3F capacitance and about 50mOhms.
We would have expected, that the output voltage raises within about 2 seconds to 5V (at current limit) and then stable 5V is continuously available at the output.
Instead of this the output voltage increases very slowly - within about 20 seconds - to 3V and then raises with about the expected rate to 5V. Once 5V is reached this is weak under load and drops to 4.2V at 3A load. If at power on an electronic load with e.g. 2A preset load current is connected the output voltage does not raise at all.
Picture 1: Circuit schematic (PDF):
Picture 2: Voltage drop by 0.8V as load steps to 3A (from no load):
red: VIN, white: VOUT, green SS
Picture 3: Startup period with very slow voltage increase:
Any ideas what's mistaken and how to solve this (or what additionally to check).
Kind regards
Arndt