Dear Colleague,
In the case of multi-chip cascade, chip 2 transmits protection action by receiving CHGU/DSG signal of chip 1. Under normal circumstances, the high-level output of CHGU and DSG pins of chip 1 can be detected by the CTRX of chip 2, so chip 2 can be judged that chip 1 has no protective action. However, the CTRD and CTRC of the chip 1 are connected to the ground, which is the same as the signal that the chip 2 receives when the chip 1 is protected (CHGU/DSG is low). In both cases, the inputs are the same, but the output is different.
So how to explain this logic?
Thanks a lot!
B.R
Rock Su