I am working on a high-power, DC-DC converter application, and planning to use the LM5176 IC to drive the control(s) for this converter. Given the high power, 20-40V @ 50A application, I was looking to interleave 2 phases together - with each phase being 180 degrees apart. Output is nominally 30V, and so buck-boost functionality are both required in this application.
However, in looking at other Power Management forums, this "master-slave" configuration of two LM5176 ICs may not be supported or functional. Can anyone shed light on this for me? Will these work in a master-slave configuration, for 2 interleaved phases? Or should I be looking at a different control IC.