This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USE OF PULSE TRANSFORMER

TIDU 248, Pulse transformer used to couple drive with high and low side mosfets.  input signal, output of IC 27324 is used as sum of the two signals A+B, being given to high side and low side mosfets. This scheme seems erroneous, as it is likely to shift the turn on level of high side mosfet.  Dead bands of each side shall be lost.  high side shall be turned on turnoff time of low side mosfet.

the scheme may kindly be explained.  

Thanks and Regards,

AJAY SABHARWAL

EVERON ENERGY SYSTEMS PVT. LTD.