This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS57160-Q1: TPS57160-Q1 Web bench frequency limit

Part Number: TPS57160-Q1

I am doing a quick look in web bench and it is arbitrarily limiting the switching frequency.

design inputs are 20V-30V with 12V output @0.5 amps.

Per the datasheet, section 8.3.12 Selecting the Switching Frequency. I should be able to get much higher frequency.

Looking at the minimum on time vs duty cycle I should be able to switch at relatively high frequencies, I just want to make sure I am not overlooking some limitation of the part.