Other Parts Discussed in Thread: LM5067,
Hi TI,
I'm using hot swap controllers in my schematic.
The power supply is 32~60V at 20A, and output capacitance is 390µF.
My problem is it can not start even 1A load because of OCP.
When I moved to output capacitor to infront of sensing resistor. It can start well at full load range.
Is it normal? I attached waveforms of CS pin.
#1 CH4: VSENSE (pin5)
#2 CH4: VSENSE (pin5)
Parameters
1.input voltage: 32~60V
2.Output current: 20Amax
3.Rs: 1.3mohm
Please let me know any side effect when I moved capacitors.
Thank you