Hello,
We are using the LMG1205 to drive an EPC2108 and are seeing that the HO gate voltage is collapsing when the our load is switched on. This can be remedied by increasing the bootstrap capacitor to about 650nF.
We are pulsing the system at 20% on 80% off, at a low freuency of 10kHz. The on pulse time is actually about 19us.
This has resulted in examination of the bootstrap capacitor value calculations and some questions:
1) In the bootstrap cap equation, why is the quiescent current of the high side driver used instead of the maximum current value?
2) I am aware from background research that HB to HS leakage current is possible and it seems this could be contributing to the problem. Is there a way of quantifying this?
Kind regards
Matt