Hello
LCD application ,VDD=3.3V, AVDD=13.28V,VGH=22.09V, VGL=-7V; VGH with one charge pump stage.
Fault: it seems could start-up sucessful at the begining, but after 5S, the VGL and VGH go back to 0V, but AVDD is OK just with some ripple; then after 8S ,VGH and VGL try regulating to its target voltage but failed. detail waveform could see in the attached .doc.
At first, I think it may be caused by overload on VGL or VGH,lead to TPS65150 enter in shutdown for out-of regulate protection, but I find AVDD is normal just with some ripple ,so it could not be enter in shutdown.
Secondly, it seems not to be in UVLO ,because of boost converter was working.
So do you have any comment here ?
by the way , today my another customer also find one set TPS65150 board have similar problem, Engineer repeately power ON/OFF VDD 3.3V, some times the board could be start up sucessful,some times it couldn't, the AVDD is ok, but VGH,VGL could not start-up.