Other Parts Discussed in Thread: LM5121
Vin is 27 to 55
Vout is Vin to 65
Lin is 4.1uH
Rosc is 43K or running about 208Khz
Cout is 10,000uF
Inrush limiting works fine, safely charging Cout to Vin, However Boost operation above Vin does not work.
One pulse on LO pin, and chip resets itself and cycles itself continuously at SS or RES rate. Cout never charges above Vin.
Schematic follows: