Other Parts Discussed in Thread: PMP20497,
Dear Sir/Ms.
I refer the PMP20497 to design the power solution.
http://www.ti.com/tool/PMP20497
Vin: 12V~56V
Vout: 55.5V/1A (system load 0A~0.6A)
Can I remove the Flyback transformer auxiliary winding?
Because I remove D2, the system seems work normally.