This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
IC: MC34063A
Input: 24V
Output: +-12V
Current: 200mA
Question: Kindly provide a reference design for the above application if possible!
This IC selected due to cost. Also don't want to use discrete components.
Note Web Bench seems not working for this IC! Like to simulate in Web-Bench but not able to do this online.
Power source is Wall Wart, 24V.
Neil Henry
IRAD LLC
Hi Jasper,
Ground isolation is required. All option is in consideration. Cost is a driver though.
The client wants to use Wall Mount AC adapter such as WAU12-200.
For the headphone amplifier, the design team selected the TI LM4562 and or LME49720, or the OPA2134.
For me the NE5532 and RC4580, with load 600OHM should be adequate. So we are looking at all options.
Since noise is an issue, ground isolation key to the design, the main driver.
Thank You,
Neil Henry
IRAD LLC
Hello Jasper,
I found this reference design PMP7006 for the IC MC34063A.
I would like to modify it for our objective, plus and minus 12V. Client will delete the 9V battery requirements.
Can you recommend a viable T1 for this design, since the WE 760370102 not on market. Looking for an alternative part number.
Thank you.
Neil