Part Number: UCC28780
Other Parts Discussed in Thread: LMG5200
Seems UCC28780 active clamping device is the LMG5200
If the input is approx 380v, would this device be useful?
I do have control over this dc input.
It comes from a PFC working on a 3phase ac bus.
What would be the optimal output to use LMG ?
Another question then is : what gains one will have in efficiency if we use MOSFET? There are plenty with excellent performance as well.
r