This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54240-Q1: productiveness

Part Number: TPS54240-Q1
Other Parts Discussed in Thread: TPS54240

We had some problems using TPS54240, so please look at the input: 12? 36V output requires 5V? 2A, actual measurement, Low efficiency (tested at input voltage 12V) 1A efficiency 78% 0.5A efficiency 82% 1.5A efficiency 50%