This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM34910C: 48V input,12V output 800mA problem

Part Number: LM34910C

I maked design as shown datasheet and app note prefered. So SW pin signals is ok. FB has a problem. IC going to safe mode or OVP mode i think.

I searched, 2 people has same problem. Maybe this is design problem. I tried many recovery diodes, same problem.Diodes Vf 500mV to 900mV

first way to work, lower inductance, my design has 100uH, when i used 47uH it works but coil going to heating.
second way to work, adding 2" cable to recovery diode and place near the coil. that will work. I checked signals, fb pin has a distortion when sw fet working.

I used many type of diodes, Vf about 500mV to 900mV, series. Also i tried current sense resistor, 680mR and 330mR, and shunt the current sense. this is FB pin problem.

Any one try to help?

  • M.Yuksel,

    Do you have a voltage on the output when you start up the LM34910C? If so, this thread details what is happening. In short, the part may not start in a pre-bias condition.

    If not, please give me a detailed list of your test setup. What are the voltages on the pins for your sequence before, at, and after the issue you observe.

    -Sam