Part Number: BQSTUDIO
Other Parts Discussed in Thread: BQEVSW,
It appears that I can load most of the configuration, system data, gas gauging, Ra Table values from my golden image, but it doesn't appear to update any of the calibration data values stored in the golden image. Is this area protected? Do I need to change a preference in my bqStudio in order to import calibration information into data memory? The old bqEVSW allowed the golden image to import all data flash values including calibration values (CC Gain, CC Delta, CC Offset, Board Offset, Voltage Divider, etc). How can I get these calibration data memory values to update when I use "Import from file"?
The old bqEVSW seemed to change CC Gain, CC Delta, CC Offset, and Voltage Divider when running just the Voltage calibration. The bqStudio software seems to only touch the Voltage Divider value. Is this true?
Do I need to perform CC Offset and Board Offset calibration steps in addition to the Voltage calibration step?
I tried to post these questions on TI's Customer Support page (Case #CS0020311) but the only reply I got was that they didn't know and that E2E community was my best option for answers.
Jeff.