Tool/software: Code Composer Studio
Thanks for your answer about timing of erasing data!
However, do you know answers of other questions about reason of I2C hang ?
1,In order to solve gost current problem, I increased cc deadband from 17 to 68(The cc deadband of V04 was changed to 68.) according to your advice. Is cc deadband change stored in 'Instruction flash' or 'Data flash'? In fact, I had been told that dffs file can cover cc deadband change during time of solving this issue? Could you confirm?
2,Our factory will buy BQ27510-G3 from TI and update it via V04 dffs file(it is attached). Could I update FG using V04 dffs file without any our configuration data loss because dffs file doesn't include IF section without any our configuration data loss? Is IF part of V04 bqfs file same with default IF part of G3 bought from TI? Would you help confirm it is ok to use V04 dffs file?
3,What steps are needed to update FG via dffs file and bqfs files? Is this process same?