Hello,
I am using UCC28780 for my Activ Clamp Zeta-Flyback Converter. The Output Power of the Converter is 160W (40V and 4A) and i already used your UCC28780 Si SIMPLIS Model (45W Output Power) for my Simplis Simulation and adjusted the circuit parameters with help of your e UCC28780 design calculator for my Topology and Output power. In Simulation everything worked well. Now I built a Hardware and have a Problem that the Controller doesn't start. The Start Sequence with the SWS, RUN, VDD HVG, works propertly i measured on every pin. The only thing is the main Mosfet Ql (Ql name in your SI Simplis Model) Switch only ones or sometimes twice and stops until the VDD Capacitor is Empty and a new Start Sequence starts. My Primary inductivity is 75µH and Input voltage for C bulk is 250 V (DC). Can you help me with this Issue?
Thanks!
BR
Ivan
e UCC28780 design calculator