Other Parts Discussed in Thread: CSD95372BQ5M
TPS53641 has VR_FAULT# asserted low. the fusion shows VIN_OV_FAULT_LIMIT (register 0x55) to be 15.000, with HEX value of 0x000F.
This is the only item that is different from a good working controller which shows VIN_OV_FAULT_LIMIT(register 0x55) to be 17.000, with HEX value of 0x0011
As a result of this failure the output voltage is at VBOOT value, and VOUT_MAX is at 3.04V (0x00FF).
Since I don't know what has caused this over voltage, I compared all pins voltages with the good working controller. The only difference that is see
is with pin TSEN (pin 40). the failing controller reads 0.833 volts, and the good controller reads 0.887 volt.
The input to TSEN is wire-AND of TAO output of two regulators(CSD95372BQ5M), as this controller has two phases connected to these two regulators.
Would you please instruct as what could be the issue, and your recommendation on resolving it.
Note. FUSION shows the IMAX, value to be 55A, the same as good working board. I have checked all items listed in FUSION's General, Advanced, Device_info, and All config
to be the same as good working controller except the one mentioned above.
Thanks,
-jahan