Hello,
The Pout(max) in the table 5 of Buck Boost design parameters is 12.6W.
However, the Vout is 39.6V(max) and ILED is 1500mA(max). So the Pout (max) would be 59.4W
I think that the calculation of Pout is not same with 12.6W if we use maximum value of Vout and ILED.
Is the calculated value of 12.6W correct?