This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: Conversion time for coloumb counter ADC

Part Number: BQ4050

Hi,

I have 2 questions:

-------------------------------------------------------

1-

The load current profile is square wave of  200mS with 5% duty cycle. 

On time = 10mS@2mA

Off time= 190mS@1A

 -> Average of 190mA.

Would the bq4050 be able to measure current (and as a result count properly the coulombs), when there are such narrow pulses ?

-------------------------------------------------------

2-

In the datasheet, table 6.17, there are 4 lines for single conversion time. what does it means? Can i configure the conversion time?

-------------------------------------------------------