This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: FC not set at the end of charge

Part Number: BQ34110

Hello,

I'm using a Nimh dT/dt as event for end of charge detection. (I'm using the FC bit to stop the charger.)

I had a strange issue that I didn't had previously: at the end of one charge, the FC didn't set and I overcharged my battery.

Is it a bug or does something in my configuration prevents the FC bit to be set at the dT/dt event?

(I attached the datalog file and the last gg.files from the autoexport)

 datalog.zip2084.datamemory.zip