Part Number: REF5025
Hi Team,
The datasheet says the ESR of CL must be less than or equal to 1.5Ω to ensure output stability. My questions are:
1. Why ESR with 1.5Ω or less is required to ensure output stability?
2. What if the ESR is higher than 1.5Ω?
3. At which frequency range should the ESR be 1.5Ω or less?
From the block diagram, the Vout is from an amplifier, usually the phase margin of open loop gain is big at low frequency. The ESR of capacitor at low frequency such as 2.8Ω @100Hz is also higher than 230mΩ@ 1KHz. Does it mean that the ESR should be less than 1.5Ω from 100Hz to 10GHz or just at 1kHz?
Thanks and Best Regards!
Hao