This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: PCB issue

Part Number: UCC28950
Other Parts Discussed in Thread: PMP8740

Hi,

It is written in the schematics that Disconnect the anode of D25 from the ground and connect it to the anode of D18.

But the thing is that in the CAD file the connection of A-D18 is not there.

So which one I have to follow, the actual available connection in PCB cad file or the one you have mentioned as a note?

What is the importance of this A-D18 connection in a precharge circuit?