This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
My schematic is attached.
Questions 1:
Per section 8.3.6 TI recommends that a fet with 1nF Ciss or greater is used. I'm referring to the first of the three bullet points. My load is very light and because of that I'm using the PMPB215ENEA N-Channel FET. This has a Ciss of ~215pF. What should I do to make sure my TPS2412 is stable and operates correctly with this FET?
Question 2:
Per the second bullet in section 8.3.6, does every TPS2412 circuit require 100uF ceramic output capacitance? I'm wondering if I need to add this as my load is very light (basically an MSP430FR5969 and some peripheral digital circuitry). Right now my output is 4.7uF which is way off according to this statement in the datasheet.
Screenshot of the bullets from the datasheet I'm referring to.