TPS65381A, data sheet, page 8, (4):
"Under slow VBAT ramp-down and when VDD3/5 rail is configured as a 5-V rail, the NRES output can be pulled low when VBAT is at
approximately 6.3 V. This occurs because of an undervoltage transient on the VDD3/5 rail. "
why could this situation happen?
CAN net must be operational when power supply is as low as 6V in automotive circumstance.