Hi,
The charging temperature range on the bq24616 datasheet is 0C to 60C with the charge current dropping to 50% between 0C to 10C. My battery can only charge from 0C to 45C. Will the charge current still drop to 50% (2000mA/2 = 1000mA) between 0C to 10C if I set the max temperature to 45C?
The battery data sheet specifies that the battery charge at 0.35C (0.35 x 4400mA = 1540mA ) between 0C to 10C. I'm changing the range max to 45C. I'm concerned that the 50% charge current drop will happen for a range smaller than 0 to 10C. If so, then the charge current 2000mA will not drop below 1540mA at the batteries' specified range.