Which is the current limit of TO3 package without dissipation if I have input voltage of -4.25V and output voltage of -1.25V.
The Vin-Vout<15V so the current limit in the datasheet is between 0.5A and 1.8A.
With thermal dissipation of 140°C/W and with minimum current limit of 0.5A the deltaT between junction and ambient that I have is 140°C/W*(4.25V-1.25V)*0.5A=210°C
Thank you for your support
Francesco B.