This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5907: Looking for alternate due to output capacitance limitation

Part Number: LP5907
Other Parts Discussed in Thread: TPS799, TPS735, TPS734, LP2989, TPS7A90

Hi,

I was planning on using a handful of 3.3V LP5907 regulators for a mixed signal design, and have discovered that due to the 10uF output capacitance limit, there are a few instances that I cannot use this regulator. This is due to the capacitance requirements of the parts the reg will be powering (couple DACs and an ASRC for example). 

The input is 5VDC, output 3.3VDC and max current is 150mA. Need to allow for at least 30uF output capacitance. Ideally with similar noise and thermal characteristics to the 5907.

Can you suggest an alternate LDO for this application? 

Thanks

Ian