Dear Specialists,
My customer is considering BQ25703A and has questions.
I would be grateful if you could advise.
---
(1) The LSB of battery discharge current detection (ADCIBAT) is described as 256mA,
This value is defined when the detection resistance RSR is 10 mΩ.
If RSR is 20 mΩ, will the LSB be 128 mA?
(2) The RSNS_RSR register settings has 10mΩ and 20mΩ.
If the RSNS_RSR register is set to 10mΩ and the actual resistance value is 20mΩ, the LSB will be 128mA,
Or when RSNS_RSR is set to 20 mΩ, is the LSB change to 256mA?
(3) In addition, if IBAT_GAIN iresister is changed, will the LSB be 256mA?
---
I appreciate your great help in advance.
Best regards,
Shinichi