Other Parts Discussed in Thread: BQ24650
Hi,
We are using BQ25703A in order to charge 4S11P lithium-ion battery pack.
Currently the input source is an 80W solar panel (Vmp=17.7V, Imp=4.52A) and it is working fine.
In the datasheet the recommended input current sense resistor is 10mOhm - up to 6400mA input charge current.
We are wondering if we can replace the input current sense resistor to a small value like 5mOhm so we can use higher current input source (bigger solar panel).
(Same question on the battery charge current sense)
BTW, if it can be done we will replace the mosfets and inductor to fit to the new design.
Thanks,