This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24610: BQ24610: Migration from BQ24610 to Bq24630 bis

Part Number: BQ24610

hi,

sorry for the delay, I was waiting for more feedback.

I attach an excel file about my battery cycle. please follow the link (size 23MO)  https://transfernow.net/10kfn2o18q7u

battery specification : 21V 5A/h

current load : 4A

you can see on it fluctuation of the charging time. I don't know what's append and I would like an issue.

sometime end of charge after 30 min, other more.

I have another PCBA with the same design and component without any problem.

if you have more question, don't hesitate to contact me.

Kind regards

raphael MARC