This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi James,
Yes the part will have a cycle by cycle current limit therefore it will limit the peak current during an overload or short condition. Each cycle the switch current and internal COMP voltage are compared, when the peak switch current intersects the COMP voltage, the high side switch is turned off. During overcurrent conditions that pull the output voltage low, the error amplifier will respond by driving the COMP node high, increasing the switch current. The error amplifier output is clamped internally, which functions as a switch current limit.
If the IC heats up during this cycle by cycle current limit, then the thermal shutdown will kicks in and shut off the operation of the IC until the junction temperature cools down to typical 160 degree C then it try to restart again.
Thanks
-Arief