This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22990: Calculation of CT capacity

Part Number: TPS22990


Dear Sir or Madam,

I am trying to determine the value of CT using Equation 1 of the data sheet (JAJSCB8C) to adjust the rise time of TPS22990.
However, the data sheet (JAJSCB8C) says “An approximate equation ... when VBIAS is set to 5 V”.
Is it possible to use Equation 1 as it is when using at VBIAS = 3.3V?
Redards,
Hasegawa