This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54302: Getting problem in practical implementation and IC damaged

Part Number: TPS54302

Hi 

I have a requirement of 4.2V , 3A that is why i have chosen TPS54302 chip.

I have tested TPS54302 chip and IC damaged immediately.

Vin=24V/12V

Vout= 5.14 V

C1= 10uF

C2=0.1uF

R4=200K

R5=100K

C4=C5=22uF

R2=100K

R3=12.7K

I have provided input voltage 12 V but the IC damaged immediately.

In first case EN pin is open

In 2nd case En pin is connected to resistor divider network 

Output received 3V but IC got damaged immediately 

I have only 2 samples left now.

Still not received satisfactory result. 

Help require.

Thanks 

Pallavi