Other Parts Discussed in Thread: LM73606, LM73605
I am concern about light load condition in my design and want to avoid pulse skipping mode of operation due to light load. From the datasheet i am only getting the statement as below
In page no 35 of datasheet - With an input voltage of 12 V, the example design enters discontinuous-conduction mode when the output current is less than 408 mA. The power supply enters Eco-mode when the output current is lower than 25.3 mA. The input current draw is 257 µA with no load.
but for my design How to estimate this boundary limit.
Thanks & Regards,
Suriya R