Is there a minimum threshold for the amount of current this device can limit? For example could I set Rcl = 40kohm to set the output current limit to 50mA (0.8*2500/40000 = 50mA)? Is there a upper limit for the Rcl value? What is the effect on current limit accuracy larger values of Rcl?