Hi,
If I am going to change the output voltage level to 75V maximum, do I need to change the Diode ratings of D23 and D25?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
If I am going to change the output voltage level to 75V maximum, do I need to change the Diode ratings of D23 and D25?
Thanks.
Hi Nidheesh
I'll have to check this with the designer - please be patient.
Regards
Colin
Hi Nidheesh
I got a reply to your question just now.
"The switch-node “PH” pin 3 of U6 is used to create a floating voltage (V-FLOAT) that supplies the gates of high side back-to-back FETs.
Since this is a floating voltage, D23 and D25 will have the same rating (they “see” V-FLOAT” voltage, which is, worst case, 15V).
The 75V will drop across C72, since this capacitor removes the DC component."
Regards
Colin